Dear Sir,
In TPS25200 datasheet, page 4, 7.3 session- Recommended Operating Conditions, the TJ is -40 ~ +125degree, But the OTSD1(135 degree) or OTSD2 (155 degree) of thermal sense is greater than +125 degree, if TPS25200 is in output short, any risk for customer?
And in 7.1 (Absolute Maximum Ratings), it says tht the Max. TJ (operating junction temperature) is internally limited, NO clear data, can you provide this data for customer reference?
Now when customer do the output short test, the case tempereaure is about 124 degree.
Regards,
Jack