Other Parts Discussed in Thread: LM5060
Hi,
I want to limit inrush current to my board which has 2200uF input capacitance and is switched on by a relay. I've selected the TPS2491 for this task. My intention is only to use the enable and gate drive functionality of this IC (I prefer not to include a sense resistor) so I shorted SENSE to VCC and Timer to GND. In order to limit the current I've connected a capacitor (with series resistor) to the GATE output pin.
This works great, the output voltage ramps up as expected. However when I do a tolerance analysis on the dv/dt I am a little bit confused therefore a few questions I hope someone can answer.
Q: The datasheet claims the gate sourcing current is 15uA - 35uA. Your design calculator spreadsheet mentions 16uA - 28uA. Which value should I believe?
Q: there is a significant temperature dependancy for the gate sourcing current. Is it already incorporated in the numbers above? Or should it be added for worst case calculations?
Q: Is the sourcing current range a TI production tolerance or a life-time tolerance? In other words, can I measure the value during my production phase and compensate for it one time and then only account for temperature influences?
I hope someone can shed some light on these items.
With kind regards,
Jasper Keuning
FYI,
input voltage is up to 40VDC
I want to be able to draw up to 16A from the 40VDC after the system has booted