Im looking to find a suitable TI product that will help me with my below detailed application.
I'm developing a repeater type of equipment on ethernet (100mbps) that will sit between a PoE enabled Switch and a PoE device, both of which are standard equipment in their respective category. However I need to extract power for my HW from the PoE from the Switch, and a method to inject it on the output of my HW to enable the PoE device connected to draw it's power. I understand that a straight forward method would be to use a PoE PD module at the input and a Power injector module at the output. Im looking to see if there's a more efficient way to allow power for both devices (amount of combined power will be within the 15w limits) without using a delivery module and an injector module separately. Does TI recommend any such solution? Attached image which gives details of the requirements.
Thanks,
Ganesh K