Hi
We are going to use TPS2491 with the following condition.
(Vin=24V , Iload= up to 3A(typ)) --> Rs=15mohm, CT=0.1uF
External FET : RSD100N10
Should we set the power limit if we need to be concerned SOA of FET? (The current limit only needs but also the power limit needs?)
We had tried to evaluate TPS2491 with above conditions and no power limit(PROG is connected to VREF via 47kohm.).
However it does not work under SOA of FET.
Regards,
Koji Hamamoto