Referencing the datasheet, pages 20-21 and Figure 32, regarding the Power Up Sequence:
In Figure 32, there is a time period between t1 (Insertion Time) and t2 (In Rush Limiting), where the FET gate is charged with the 22uA source, and the text reads "the GATE pin then switches on Q1".
I have the following questions with regard to this time:
- What is meant by Q1 switches on? Is it when the Miller capacitance is fully charged? Is it when drain current starts to flow?
- Is current limiting / power limiting happening during this time?
- Does the fault timer start at the end of t1 or the beginning of t2? Figure 32 shows that the fault timer starts at the beginning of t2, but just want to be sure.
- If the fault timer starts at the beginning of t2, how does the LM25066A know that Q1 is turned on and that it should start the fault timer for t2?
Thank you,
Chris Arntzen