dear Sir
Do you have any document to describe below output diode's function
If have the waveform ,it will be better
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kai,
The purpose of the TVS diode and the Schottky diode is for IC protection. We recommend all designs with hot swap controller to have a TVS diode on the input and a Schottky diode at the output (for transients).
All wires have trace inductance and in the event of a hot short or severe overcurrent, those wires could produce a huge change in voltage at the input and output, which could damage our IC. I recommend the B380-13-F Schottky diode and make sure the TVS diode clamps the voltage lower than the abs max of the device at the worst case clamping current.
Best Regards,
Aramis P. Alvarez