Hi Ti,
Over voltage, under voltage and polarity protection is tested fine with LM5069MM-2 but when connect the output to the load that takes more than 200mA the IC is not functioning.
The design of the schematic is based on the calculation from the datasheet. Based on the datasheet the Rpwr is power limit resistor but seems it has no effect on the output current. Also changed Mosfet to a lower RDSon but it doesn’t help as well.
Can you please advise what is other possibilities to look into on resolving this problem?