Other Parts Discussed in Thread: LM5060, LM555, DRV104, DRV103
I have a 24V resistive heater drive application that may either use hysteretic (thermostat) control or a PID loop utilizing PWM drive. Since the mass being heated has a thermal time constant measured in seconds, the PWM frequency can be low, perhaps in the 10's of HZ. The LM9061 appears to be a low cost solution for driving a high-side N-CH MOSFET with controlled slew to minimize electrical switching noise. The datasheet Application bullet on the first page mentions PWM DC motor driver, but no PWM application info is presented.
Since this is a simple, non-capacitive and low-inductive resistive element load of up to 2.5Amps, there will be minimal cold-inrush so I assume the delay timer can be minimal. My understanding is that the delay timer has no effect on the ON-OFF times of the MOSFET, so I can just use the recommended non-specification Cdelay value of 0.1uF
Are there any PWM application examples I can examine and/or any particular points about this chip that I need to pay attention to? The MOSFET I choose will be appropriately sized for the load current and as long as I don't alter the gate drive, I expect the repetitive transient power dissipation through the switching slews should stay well within the SOA rating.