Hi
Can you suggest IC with below feature, application
Application :- Will be used in UPOE PSE Device (Power on Ethernet)
Port :- Can Support up to 4 Port
Type:- UPOE type ,where each Port source 60W ( or as per UPOE standard)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Can you suggest IC with below feature, application
Application :- Will be used in UPOE PSE Device (Power on Ethernet)
Port :- Can Support up to 4 Port
Type:- UPOE type ,where each Port source 60W ( or as per UPOE standard)
Hey Kunal,
The TPS23861 is a 4-port device that supports UPOE. In order to supply 4 UPOE ports, you will need two TPS23861s, as each UPOE port requires two ports from the PSE.
Alternatively, you could use a TPS2388, an eight port device that can support up to 4 UPOE ports. This device will RTM soon. Please send me your email address and I will send you a copy of the TPS2388 datasheet.
Thanks,
Jake Smith