Hello,
Very urgent ! The customer wants to know whether the resistance of the UVLO in the picture is right or not and how to choose the proper resistance.
Thanks and best regards,
Erin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Very urgent ! The customer wants to know whether the resistance of the UVLO in the picture is right or not and how to choose the proper resistance.
Thanks and best regards,
Erin
Hello Erin,
To answer the customer's question, yes, this is the correct resistance to allow for the UVLO resistor divider to also be used for detection; however, I would NOT recommend this configuration.
It is better to place the 24.9k ohm resistor from VDD to DEN and use much larger resistor values (as large as possible) than what is shown in that figure for the UVLO pin. Be sure to pick a divider ratio that provides the correct voltage at the UVLO pin according to the table on page 4 of SLVS646A while satisfying the customer’s intended turn-on (max 42V) & turn-off voltages (min 30V).
Thanks,
Thomas A.