I used the TPS23754 reference design for a 12V , 2A output. But the POE circuit can only provide about 15W when I use a Trendnet POE+ switch. As soon as I increase the load, the PSE cuts off the power. When I use a simple POE+ injector, I can draw the whole 25W. So I'm assuming the issue is with class detection. I am trying to probe the VDD-VSS to see the startup wave from but the PSE doesn't bring the rails up when I have my Tek P5050 probe connected to VDD-VSS. As soon as I remove the Probe, the rails come up.
1. I have the 63.4 resistor so why isn't my device classifying as type 4?
2. Do I need a specific probe and probing technique for analyzing the VDD-VSS?