Other Parts Discussed in Thread: TPS23753
Tool/software: WEBENCH® Design Tools
I would like to design a PoE powered device which can also powered from an auxiliary power input.
I have the following spec:
Vin = 12...56VDC
Vout = 12VDC, 1.0A
Isolated min. 1.5kV
There is the WEBENCH® Designer for designing your own DC/DC converter. This tool is great.
Can I use the tool also for the LM5071?