Other Parts Discussed in Thread: TPS23861,
Hi Penny,
I would like to develop a 1-port four-pair power injector using two of the four outputs of the TPS23861 or TPS2388.
I have questions about PSE and PD compatibility testing.
As far as I know, PD knows that there are LLDP(1-PD) and FORCED(2-PDs) methods.
Do you need an MCU to satisfy the two methods?
Do you need to control using semi auto mode?
If control is needed, do you need to control only the LLPD method?
In case of FORCED method, it is not necessary to control because there are 2-PDs.