I have an application where I need to power the router and a camera that share the same gigabit ethernet connection. Is it possible to power both devices? How do I isolate the devices from the Ti 802.3 chip power?
Thanls
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have an application where I need to power the router and a camera that share the same gigabit ethernet connection. Is it possible to power both devices? How do I isolate the devices from the Ti 802.3 chip power?
Thanls
Hi,
I’m trying to power 2 devices of the ethernet connection. Router on one side and Camera on the other. Same physical ethernet so Power Supply in the middle powering both ends. Does this make sense?
I also have one other connectivity question I'm planning on using the attached ethernet jack with PoE magnetics embedded. Can you please let me know the proper pins to connect to the TI PoE Power Supply chip?
Thanks
MarkLPJ0012GDNL.pdf
7824.LPJ0012GDNL.pdfsorry wrong eithernet connector. this is a gigabit which is my choice. Thanks
Hi Mark,
How many PSE channels and PD controllers do you want to use?
If the total power of router and IPC is within type1, it is possible to use a single PSE channel and a single PD plus flyback controller with two different outputs which can also realize isolation from PSE side.
If the power is larger, you can use two PSE channels with two PD controller including two flyback controller to supply power independently for routers and IPC.
Thank you.
Best Regards
Jack Chen
Gig_RJ45_Magnetics.pdfThanks for the info. So if I understand this correctly I can use 2 channels of the TPS23861 chip one for thr Router and one for the IPC and I can have PoE+ for each device? My plan is to use 2 channels one for each device. Do I need to provide any isolation between the data conductors between the RJ45 with built in magnetics?
Can you help me with the wiring to my Ethernet jack which has built in magnetics. I am attaching a schematic of the connector. I'm not quite sure which pins to connect to the output of the TI TPS23861 chip. I know the chip suplys ( + & - ). Do I connect all of the +'s and -'s to the 2 pins of the chip. I see that on the data pins on the PCB board side are clear, do I apply my +48v (supply) to the VC+ and VC- or is that the output from the TI chip? and what do I connect the MDCTL1-4 pins to?
Thanks for all the help