Other Parts Discussed in Thread: TPS23752, PMP8812
Hello,
I would like to design a PoE PD with the following specifications using TPS23751.
・Vin(min) 36V
・Vin(max) 57V
・Vout(Nom) 24V
・Iout(max) 1.25A
・Class 4
・Output Power 30W
・Isolated
・Input Type DC
・Topology Flyback Converter
Is there any 24V output reference design?
What is the recommended product of 24V output flyback transformer for TPS23751?
For example,POE300F-24L(Coilcraft)?
Best regards,
Seishin