Other Parts Discussed in Thread: TL431, , PMP8803, TLV431
Hi,
We design an 802.3at PD with 12V output. I suffered from a reliability issue that 15% of the PDs will malfunction within
2 ~ 4-month due to damage of TL431 (in SOT23-3 package). The output of PD is used as power source of consumer apparatus
which are not inductive and consumed around 10 ~ 15-Watt. We did experiment by shorten the output of PD to
emulate over-current. The results show that over-current protection scheme of LM5072 will be activated and there is no damage on TL431.
The PD design is based on the reference design of LM5072 for 802.3at. Do you have any clue?