Other Parts Discussed in Thread: LM1086
I am not that familiar with switching power supply circuits. I have found the following schematic for a PoE device:
http://www.ti.com/lit/df/slvrb18/slvrb18.pdf
with the output of 5V @ 4.8 A.
However, I need a voltage level of 6.5 V with lower current.
My questions are:
1- How can I change the circuit to get that voltage level at the output?
2- Since this PoE output is Mode 2, do I need to do extra things to make it work? (In the documentations a Data Link Layer (DLL) classification is also mentioned for Mode 2 PoE devices).
Cheers.