Hello,
What limits CSD87352Q5D switching frequency to 1.5MHz, could it go to 2 MHz?
Power Blocks can operate at 2MHz.
Jeff,
Thank you. What is the maximum switching frequency?
Additional Questions from the customer.
Is the fact that the switching frequency is listed at 1.5MHz and not 2MHz, due to the device not tested at 2MHz.
Driver chip for the NextFET TPS28225/6 is capable of 2 MHz. Is more verbose explanation available on gap between 1.5 and 2 MHz?