• Resolved

CSD95373AQ5M: CSD95373AQ5M Θja(°C/W) infromation

Part Number: CSD95373AQ5M

Hi All,

Please kindly help to share Θja(°C/W) infromation to us.

It haven't fill in datasheet. thanks.

Thanks.

  • Pao,
    The case to ambient thermal impedance for any device is generally more a function of the board and the thermal environment than it is the device.

    For a 5x6 QFN, 1" 2oz Cu yields an RthJA of around 40degC/W. When using the min possible copper, this value is closer to 100degC/W. It application, it could be anything in between, or even down to 10-20degC/W depending completely on your board, how and if you heatsink, etc...

    Brett Barr

    Product Marketing Engineer, Mid-Voltage FET