This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

P-Channel 4 terminal Mosfet with Body

Hello Sir/Madam

I am looking for four terminal P-MOSFET with body terminal. In my application i need to adaptively bias the body based on S/D , whichever is higher. Could you please point me to high voltage four terminal P-MOSFETS.

Voltage ratings specification ( if not available for this specification, any 4 TERMINAL power MOSFET with lower ratings is also fine):

-Used as load side switch in Boost converter.

- Max source voltage 30V

- Max drain voltage 30-40V

-Max drain current 3-4A

Thanks

Sujan