Can you support us to choose MOSFET, please find below the critical parameters
MOSFET – Requirements
- Signal MOSFET-N Channel
- Application is in the active region / Implement in Linear region, so that MOSFET can work as a precision resistor
- Maximum load Current – 500mA
- Vds – 24V
- Gate Source threshold voltage – 1.5V
- Gate Input – PWM generated by uC
- Product application
- With variation in frequency / pulse width, voltage at the drain should vary
- Expected load range is 1.5V to 8V
Please let us know, if you need any further information. Thanks
If this is not the right forum, then can you please redirect??