This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NEED INFORMATION- CSD19502Q5B

Other Parts Discussed in Thread: CSD19502Q5B

Hi Can you please provide the following information for the CSD19502Q5B Part ?

1. Junction Temperature Max (Tj Max)

 2. Typical Power dissipation (Pd typ)

3. Maximum Power dissipation (Pd max)

4. Thermal Resistance Junction to Ambient (Theta JA

5. Thermal Resistance Junction to Board (Theta JB)

6. Thermal Resistance Junction to Case (Theta JC)

7. Weight          

  • Jayakumara, 

    Most of these parameters can be found on the datasheet. 

    1) Max operating temperature: 150 deg C

    2 - 3) Not sure what you mean by typical power dissipation. The device can handle up to the max power dissipation, given the thermals provided on the datasheet, which is 3.1W. 

    4) Typical 40 degC/W, Max 50 degC/W

    5-6) These parameters are a function of the amount of copper used and are entirely dependent on your board conditions and layout. Please refer to the datasheet (min copper vs. max copper) for an example. 

    7) ~100mg