Please let me know 3-points below about CDS75207.
------------------------------------------
・It is written to the datasheet as "Continuous Drain to Drain Current:3.9A".
Is 3.9A Current Value of Total Which two "Drain" Pins? (1.95A/FET)
Or is one FET the spec of 3.9A?
・About Figure2 of a datasheet. The current will also become large if the voltage of "Drain1 and Drain2" becomes large.
Is it that current flows into "Drain1 to Drain2", or "Drain2 to Drain1" according to the voltage difference of "Drain1 to Drain2"?
・Isn't usage which 2-FET controls scattering carried out to Common Source?
------------------------------------------
Best regards,
Satoshi