This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD86311W1723 ESD

Other Parts Discussed in Thread: CSD86311W1723

CSD86311W1723 datasheet note on the top of page 2:

These devices have limited built-in ESD protection. The leads should be shorted together or the device placed in conductive foam during storage or handling to prevent electrostatic damage to the MOS gates.

What prompted this note?

 Can this support the 2KV HBM? What ESD level is this device protected from?

  • Tom, 

    This note used is a TI standard that goes in all of our datasheets. 

    However, no, these parts cannot support 2kV HBM. These chip scale package devices require built in ESD protection to be able to handle voltage spikes of that level. This part is only rated for 200V HBM.