Will be using the CSD95378
This is a output stage for a switching power stage. It has an H Bridge on the output side that can drive a lot of current.
It would drive a step up transformer that would drive the current through the loop. I am 100% sure this is not what it was designed for. Can you find someone in the TI world that can discuss this design and the limitation of the part. Basically I want to switch 12v and 3 amps at 8 Khz and drive a several mH inductive load (varies as the length of the loop) on the other side of my transformer.
thanks!