The CSD95372B looks like quite an interesting part, but the datasheet is severely lacking in operational details. I see that the -A version datasheet has quite a lot more information, but the -A variant doesn't have the current sense function that the -B variant includes. So as far as I can tell, there's zero documentation available on the CSD95372B's current sense function. I don't see a transfer function for Iout vs ID, or even a recommended range for REFIN. The application schematic isn't even any help since the referenced controller is under an Intel NDA.
Could someone shed some light here, or even point me towards a similar but better-documented part?