How do we integrate this mosfet in our circuit, there are no pins to put it on our bread board
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The CSD16407Q5C is a surface mount device and would need to be mounted on a pcb, with no external leads it is not possible to effectively bread board this device and maintain a reasonable thermal solution.
You can purchase an evaluation module through TI.com at http://focus.ti.com/docs/toolsw/folders/print/csd163cevm-591.html
The EVM is populated with the CSD16322Q5C and CSD16321Q5C, these devices can be removed and replaced with your preferred choice of devices. These devices can also be ordered directly from TI.com.
The CSD16322Q5C has lead in the die attach material, similar to many power MOSFETs.
This means the device is RoHS compliant (or exempt) when using exemption 7 in the RoHS regulations that allows the use of high lead solders for die attach.