Hi,
I'm relatively new to this and haven't had the opportunity to take a class on MOSFETs just yet (soon!). I've done some research and hopefully I'm not horrifically off on this.
I'm attempting to design a motor driver using the DRV8701 in conjunction with CSD18536KTT for the N-Channel FETs.
My requirements are for a 24VDC Brushed Motor, rated at 24 Amps. Locked rotor I measured it to be about 30-35 amps continuous. The power supply I'm working with is rectified 24VAC, which ends up being around 33 VDC. This will be controlled through PWM as well.
These FETs might be overkill with respect to the continuous drain, but the other specs seem to be good. Is there a problem with me being way over the top of the Id? These FETs also have a very low Rds which is what I believe I should be looking for.
Any suggestions, help or advice is much appreciated!
www.ti.com/.../csd18536ktt.pdf
Thank you,
Mat