Hi Team,
I am working on a low side NFET driver that needs to handle a continuous current of 50A. I am thinking of using the CSD18536KCS due to its high current capability but I have a question about Vds.
Currently If I use the CSD18536KCS as a low side NFET driver the voltage drop across will be related to its Rds on (1.25-2 mOhms) x Ids (50A) which will be 100mV. My issue is that this value on the SOA curve lands above the grey line which is the Rdson limit line as you can see in the graph below. I marked this by a RED dot.
My questions are:
1. If I feed the FETs 50A what would Vds become? I have a feeling it might turn to the blue dot but I am not sure.
2. If I use 2 FETs in parallel would I get the result of the green dot because the new current is 25A?
3. What do you guys recommend in terms of a FET that can handle 50A continuously?