This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD13302W: How to use N-MOSFET as the load switch for negative voltage supply? Like CSD13302W.

Part Number: CSD13302W

Hi team,

My customer is designing the power supply circuit for AMOLED panel and want to use N-MOSFET as the load switch for a negative supply voltage (ELVSS).  application diagram as below.

ELVDD is 4.6V, ELVSS is -3.0V, VCI is 3.3V, VDD is 1.8V, VGL is -6.0V. 

we want to use a GPIO with VCI or VDD as high voltage and VGL as low voltage to control the gate of MOSFET. would you please suggest if this approach is OK? will the MOSFET be off when VGS is below 0 volt? do you have any other suggestion on this application? thanks. 

Kevin