hi
i am designing two boost converter
1. Vin= 12 V dc ,Vout=50 V dc ,I out(max)=1A
2. Vin= 50 V dc ,Vout=150 V dc ,I out(max)=.02A
Q1: Which Power transistor i have to use ? Whether any tool available for selection of Power MOSFET? (i have seen an tool for buck converter design but i need boost !!!!!!!!)
Q2: I know that Vds >1.5Vout and Rds on should be very low and Pd< 500mW (from calculation) any Power mosfet meets this criteria are available with TI or not?
Q3: can i directly go for a boost with Vin= 12 V dc ,Vout=150 V dc ,I out(max)=.02A? since it need a duty cycle of 94% whether it's possible to design?
thanks in advance
DEVITH T
Sr.Project Engineer ,
NIELIT