This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD97396Q4M: why the pins is short circuited?

Part Number: CSD97396Q4M

HI,

 I want to measure the voltage of the resistance in the RLC circuit. And I connected the 10uH inductance and 5.6Ω resistance to the P3.

Then two 5V power supply of DH1718D-4 is provided. PWM1 and PWM2 send the 100kHZ  signal and the duty cycle is 50%.

Maybe I make some mistakes. The voltage of the resistance is wrong.

I use the multimeter to measure the pins.

The pin PWM1 , BOOT,  BOOT-Rand the PGND  is short circuited . The pwm2 and the VIN is short circuited.

Then I change the DSP and the CSD97396. I have a good result .

But then I find  the pwm1 and PGND is short circuited again. And the U3 is fine.

why did these problem happen ?  And  the maximal current of power supply is 3.5A. Can  the power supply  result in the problems? 

Regards,

TIANQING LI