This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CSD95378BQ5M: Max VDD Current

Part Number: CSD95378BQ5M

Hi,

My customer is planning to use the CSD95378BQ5M and would like to know the max Vdd current in order to size their 5V supply accordingly. I do not see a spec for this or gate charge on the ds. How much Vdd current should they plan for?

Thanks,

Antonio 

  • Antonio,
    Max VDD current is 250uA during standby and typically 27mA during 5V, 50% duty cycle, 500kHz operation. You are correct, this is not on the datasheet on the web.

    Please feel free to email me and I can loop you in with the owner of this part if you have more questions.

    Best Regards!

    Brett Barr

    Product Marketing Engineer

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.