Hello Team,
I have noticed that the CSD87335Q3D datasheet on the Stencil recommendation in section 11.3 recommends a single aperture for the pin 1-2.
On the other hand, in Figure 34, is shown that the pads for pin 1-2 are separated.
Can you recommend how the solder mask should be considering that the stencil has a single aperture and the pads are two?
It looks as a mismatch between the Figure and Stencil.
Thanks,
SunSet