This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD18531Q5A: Temperature characteristics of gate charge total (10V)

Part Number: CSD18531Q5A

Hi,

Do you have temperature characteristics data of gate charge total (10V)?

Best regards,
Shimizu

  • Shimizu,

    Thanks for the great question.
    The short answer is we do not have characteristics of over temperature, this is because the total Qg varies very little over the whole temperature range of the FET, a far greater variation is this lot to lot fab variation which is taken into account with the datasheet typical and max numbers at 25degC.

    Best Regards
    Chris