Other Parts Discussed in Thread: CSD19535, TL431, TLV431,
Dear all
I will design for constant current circuit.
Please check to the circuit and advise to me
1. Condition
-. Input Voltage : DC 60V
-. Id = 250~300mA
2. Problem
1) CSD19535 FET heating (about 80~90 ℃ at 25 ℃)
-. Could you improve method(included Heat sink) ?
-. Could you recommend to Voltage reference(TL431 or TLV431)?
2) If TL431 output voltage is higher, CSD19535 Heating temp. is lower
-. For example TL 431 Vref voltage is increase.
Thanks and Br