I am looking for a power MOSFET with the following requirements: Switch 24 VDC, Max 10 Amps, Low Power Dissipation / On Resistance since it will be in a small enclosure.
We are using the RFP30N06LE from Fairchild (http://www.fairchildsemi.com/ds/RF/RFP30N06LE.pdf) - this is a TO-220 package and would like to move to a surface mount package in the new design.
Is there anything from TI's family of power NexFETs that might be suitable for this application?
Thanks in advance.
The RFP30N06LE is rated at 60 volts. The highest VDS rating on any of the NexFETs is 30 volts.