• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Power Management » Power Modules » Power Modules - Forum » DCR022405 Smoking
Share
Power Modules
  • Forum
Options
  • Subscribe via RSS

Forums

DCR022405 Smoking

This question is answered
Daniel McClure
Posted by Daniel McClure
on Oct 17 2011 14:34 PM
Prodigy20 points

Hello,

I was planning to use the DCR022405 in a design, and made a 2 layer prototype board using the circuit in figure 4 of the datasheet (with only one converter). I input 28V, and regulated it down to 24V using an LM7824. There was no load. When I applied power, it smoked.

The only differences I can see between the datasheet recommendations and this prototype are that there is no ground plane for heatsinking, and that the caps used were not low ESR. Has anyone else had a similar experience?

Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Tom Guerin
    Posted by Tom Guerin
    on Oct 17 2011 15:08 PM
    Verified Answer
    Verified by Tom Guerin
    Mastermind21350 points

    The DCR022405 is not recommended for  any application when the  input voltage is absolute maximum limit is exceeded  29V  or transient  for any duration. The input power  source during ramp-likely had a transient overshoot which exceeded the maximum voltage. The input capacitor must be a 2.2uF ceramic low ESR  or the converter will oscillate  and not function . Either condition will force the converter to be thermally   overstressed. The in-rush current can be > 500mA from the LM7824. The input voltage wire if longer with add impedance and increased transient voltage  If the LM7824 is hiccuping during power -up transition, this can also increase the  power dissipation with thermal overstress and subsequent  package failure.

    Tom

    tguerin@ti.com 

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Daniel McClure
    Posted by Daniel McClure
    on Oct 17 2011 15:32 PM
    Prodigy20 points

    Tom,

     

    Thanks for the quick reply. So you're saying that what most likely happened (if it wasn't strictly the fact that the capacitor was not low ESR) is that the regulator's output transient exceeded 29V for some period? If this is the case, how can I prevent it from happening in the future? Is it just a matter of increasing the capacitance on the output or adding a TVS, or should I just not use a linear regulator altogether?

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Tom Guerin
    Posted by Tom Guerin
    on Oct 18 2011 09:12 AM
    Verified Answer
    Verified by Tom Guerin
    Mastermind21350 points
    DCR01_02 24 Vin 05Vout USVSUVLO.pdf

    Daniel:

    Thanks for the e-mail. There are several concerns or reasons for this type of failure.

    1. The IR losses associated with long wires or small power wires plus   input power sources driven into current limit and oscillating  can overstress the converter. This power source isolation  oscillation can droop the 28V to lower voltages in the  18-13V range.

    2. The  28V input power supply must decreased to an average of 24V   to prevent voltage overstress on the  converter. The absolute maximum voltage on the 24V converter is 29V. Use the input ceramic capacitors , as recommended

    3. Add a soft start circuit  on the input sync. pin , pin 18, which is also a on-off control pin.

    Add a  soft start control circuit which will delay the start-up of the DCR022405 for 7-10 msec or until the  24V bus is actively high.This delay will prevent the activation of the 24V bus current limit  . Additional input capacitance 10-100uf  may be required to hold-up the  24V source bus during the DCR012405 active switching transition .

    See the attachement for delay and control of the on-off pin.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use