Hi Team,
In the website, plating details(Material Declaration) for part "PT78ST112S" is not given. Could you please share the same? If it is Tin plated, kindly the share the following details also
1. Type of Tin(Matte/Bright)
2. Underplating material used
3. Tin whisker test report conducted for this part
Regards
Aishwarya
PT78ST115S , PT78STXXXX series has:
1. Pin plating is matte tin(Sn) 100% 300-500 microns
2. Under plating is nickel(Ni) over a copper base metal.
3. The pins do not have any conducted tin whisker tests
Tom