This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

WEBENCH® Tools/LMZ34002: WEBENCH cannot create design error

Part Number: LMZ34002

Tool/software: WEBENCH® Design Tools

Dear Webench Team,

I am working on a design with the following requirements:

Vin= 22-26

Vout= -12V

Iout = 1A max

I did a WEBENCH with the LMZ34002 in the past and now it is saying this is not possible.  

Thanks,

Jason 

  • Hello Jason,
    I will contact the WEBENCH folks to comment.
    Regards,
    Denislav
  • In reply to Denislav Petkov:

    Hello Jason,

    We were able to reproduce the issue and are working on fixing it.

    We'll let you know as soon as the fix is released.

    Regards,

    Flora

  • In reply to Flora Carreto:

    Hello Jason,
    The fix of LMZ34002 was released today. Please try to create a design through WEBENCH visualizer.

    Regards,

    Flora

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.