This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

DCP02 SERIES ISOLATED/UNREGULATED DC/DC CONVERTERS

I have been working on designing a dual polarity power supply of no more than 20 volts or so @ 1 to 2 amps to use at my workbench at home for some time.

I found the page showing the DCP02 series and I particularly like the DCP020515DP and the DCP021212DP. The data sheet shows a fairly simple installation requiring a good connection to the input power and decoupling capacitors. I was wondering if there are some more detailed circuit ideas and applications for the DCP02 series.

  • The DCP02XXXX   are  low current unregulated ,DCP020515DP and the DCP021212DP. very low current  2W converters. The average maximum current for  each polarity is about 1W/ 12V wide ranging Vout  or 83mA  per polarity or 1W/15V 66mA per polarity. the  voltage  can range between 11.5V to 25V unloaded per polarity These low current converter   application exceeds the maximum  1A to 2A current as required .

  • In reply to Tom Guerin:

    Thanks Tom! I forgot to mention that I want to use the DCP02’s to power some op-amps used a voltage followers to boost the input impedance to a DATAQ D-194. I would also like for this power supply to be able to run several things at once. I am using a 24V center-tapped transformer rated at 2 amps and that works out to 48 watts. I have been studying the data sheets on the DCP02’s, UA78xx’s, LM317’s, and LM337’s. They talk about the advantages of using designs that incorporate voltage regulation at the load instead of central regulators having bus-bars.

    I have decided on using an LM317 in a shunt configuration able to handle several amps using power transistors as series pass elements. (Fig. 14, page 12 of the LM317 datasheet.) and setting it for 24 volts (VP is 34V). From there I will use DCP02’s for dual polarity to power op-amps and UA78xx’s, LM317/337’s to power whatever else I put on it.

    I would like to know if TI has a dual polarity IC able to handle more than 2 watts.

  • In reply to David Poston:

    David :

    There are no other dual output devices in the PLUg-in Power line with more than  2W

    The DCP022415D is capable of 2W , maximum 1W per polarity .The DCPcan be parallelled  for more current  per the  specification Figure 9. Each dual out put must have configured capacitors as per the figure 8 in the  specification . However, the inrush current per each DCP is 1x750mA .

     

  • In reply to Tom Guerin:

    David:

    My telephone number is 630-836-2828.

    Tom Guerin

  • In reply to Tom Guerin:

    Hi Tom

     

    You said that the inrush current per each DCP is 750 mA. Is this current same for all DCP02 family such as DCP021515? Also, I would like to know how much time DCP021515 can support 750 mA as inrush current? Moreover, is it possible to connect the capacitor such as 47 uF at the output of DCP021515? Is there any maximum limitation in installing output capacitor?

  • In reply to Arash Khoshkbar Sadigh:

    The   in-rush current is totally dependent upon the dv/dt of the power source.The DCP series regardless of  input or output  voltages can have in-rush current of up to 750mA. The Input  power source can be foreced into current limit during power-up duration. The power source , when in current limit,which is the DCP   longer on duration until it is at  normal operating voltage. This delay  may eventually overstress the  DCP and possible thermal damaged can occur.

    One recommendation to eliminate the  in-rush current is to:

     

    It may require  adding  a soft start control circuit delaying   the start-up of the DCp021515 for 7 msec or until the  15V bus is actively high.This delay will prevent the activation of the 15V bus current limit  . Additional input capacitance 100uf  may be required to hold-up the  15V bus during the DCP021515Uactive switching transition .This circuit  can be added to the input sync. pin,.

    I added in an attachment for delaying the start-up of the input voltage 15V, 12V  DCP series converters.  

    Tom

    DCP011515 USVSUVLO2010.pdf
  • In reply to Tom Guerin:

    Can you also let me know whether it is possible to add capacitor such as 33 or 47 uF at the output of DCP020515DP or DCP021212DP? Is there any maximum limitation of capacitance in installing output capacitor?

  • In reply to Arash Khoshkbar Sadigh:

    Arash;

    The use of a 33uF or 47uf ceramic can affect the operation of the DCP series products.  I recommend no more than 10uF low ESR ceramic capacitance on each bus.

    Tom

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.