This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

LMZ31710: PWRGD function in Parallel Operation

Part Number: LMZ31710

Hi, team.

When using LMZ31710 in parallel operation, is it necessary to connect the PWRGD signals?

Best Regards,

  • Hi Hirotsugu Kobayashi,

    THe PWRGD can be left floating if there is no need for power good features. Since PWRGD is an open drain output, if the power good feature is required, a 10k pull up resistor is necessary.

    Regards,
    Jimmy Hua
  • In reply to Jimmy Hua:

    Hi, Jimmy,

    I used PWRGD feature in Parallel Opetating.
    My question is whether it's necessary to connect PWRGD of Master and Slave in parallel operation.

    Though a sense terminal opens, is PWRGD on the SLAVE side effective?
    Is it no problem only in PWRGD on the Master side is used?

    Best Regards,
  • In reply to Hirotsugu Kobayashi:

    Hi Hirotsugu Kobayashi,

    The PWRGD does not have to be connected to both Master and Slave in parallel operation. You would only need to connect the resistor to the Master's PWRGD.

    Regards,

    Jimmy 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.