Hi,
Is it possible to adjust PTN78000W using DAC voltage?
Thanks,
Vlad
Hi Viad:
The PTN series can be controlled with a DAC. The maximum voltage which can be applied to the Rset adjustment pin is 1.25V.
One suggestion is to pre-set with a resistor to the nominal Vout in the event the DAC does not function at power up.
The one concern is the DAC voltage must be present before the module is power-up.Other wise the Vout is unpredictable . The output voltage tolerance is only as good as the DAC control voltage.
I attached note with the formula for the voltage control .
You can send me an e-mail at tguerin@ti.com for more details .
Tom