Thank you for your support.However, we do not have enough time, please recommend us to reduce mis-operation.Solution is like below.1. DC-DC Input : 12VDCWe are using Flyback AC(98Vac to 242Vac) to DC Convertor circuit.Therefore, voltage 7VDC ~ 20VDC is possible for me, so it doesn't has to be 12VDC.Flyback output ripple is 100mV p-p(without noise) when it is 12V/3A Load.2. DC-DC Output Function:Output Voltage : 1V ~ 5V VariableOutput Current : Max 5ARipple and Noise : Less than 8mVrmsV-sensing using distance : 2MeterWe found some components.LM20125LM20136LM20145LM20146TPS54550 + Si7110DNLM21212-2LM21212-2For a more confident test, we chose a few package.Please check whether these components satisfy the specification that I want.Also, if there is an application note, please recommend.