Hi,
I'm using the DCV010515D in a module (board) of my system. When I use more than 4 boards, the inrush current is so high that my main power supply module can provide enough power. My power module has 6A@5V. So, when used 4 modules with DCV010515D, the inrush current is more or less 1.5 A. How can I reduce this inrush current ? I'm using the capacitor type and value (ceramic 2,2uF low ESR) as mentioned in the datasheet and very close to the input pins.
Mateus:
Question , Are the sync. pins , pin 4 common connected?
Can you send me your direct contact number?
tguerin@ti.com