Hello,
I'm an intern at Philips Technologies in Aachen, Germany.
I'm currently troubleshooting a PCB built by a colleague of mine. He has used 8 DCR010505U. According to this thread http://e2e.ti.com/support/power_management/powermodules/f/501/t/163829.aspx , the DC-DC converters can draw up to 750mA at startup. Could someone comment on that? If this is the case, then that means I need to ensure that at least 6A are supplied at startup, which would mean I will need to replace the supplying 1A switching regulator (TL2575). This could explain, why so far the output has always been 0.
My colleague seems to have done a mistake while connecting the pins. He connected the SYNC pins together and at the end with the 5V supply voltage. How critical is this? According to the datasheet, it is only required to connect the SYNC pins together.
Any help will be appreciated.
Hamze Hachem