Hello,
I would like to connect a margining IC (Linear's LTC2970) to the Voadj of the PTH12060 to do margining control. I need to vary VO by +-15% dynamically. The PTH12060 can do only +-5% margining.
Will this work? I'm concern about messing up the stability of the PTH12060.
I will be using two PTH12060 in my design. One for +5V (+-15%) and another for +3.3V (+-15%).
Thanks!