12V module PTV12010WAH is heating up when power on.
But still it can deliver 5V to board and the load was just 1A.
Is this the expected behaviour?
Can i go ahead to load 8A?
Regards
P.Vetrivel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
12V module PTV12010WAH is heating up when power on.
But still it can deliver 5V to board and the load was just 1A.
Is this the expected behaviour?
Can i go ahead to load 8A?
Regards
P.Vetrivel
12V PTV12010WAH when Vout is 5V and1 amp load, the average power inductor temperature is about 65°C at 25°C ambient opersating temperature .
At 8 Amp load and 5Vout, the inductor temperature can be 111-120°C at 25°C ambient operating temperature. The thermal(SOA) safe operating data is:
At 8Amp load Vout =5V, Maximum ambient temperature limit is 40°C.
Hi,
Thanks for the reply.
Is it okay to have the inductor temperature of 111-125 degrees at 25 degrees?
If not please suggest the heat sink module ?
Do you have any proven solution to reduce the inductor temperature ?
Regards
P.Vetrivel
Hi :
The Thermal data (SOA) limits when operating at 5Vout at 8Amps continuously at 115°C to 125°C will affect the module long term reliability . There is no recommended solution for reducing inductor temperature at 25°C operating temperature. One solution is to increase air flow across the module .
The alternate lower temperature solution is PTV12020WAH with 5Vout at 8 amp load with inductor temps 66°C-70°C at 25°C ambient temperature.