Hello, all
Now we have some inquiries regarding input capacitor of DCP010512DB.
Please refer to the items below, and feedback us with your comment.
1) When referring page 2 of SBVA013A, the ESR requirement for input capacitor is important for stability on starting up.
However, if we could chose good ESR capacitor (less than 20mohm), the capacitance itself is higher than 2.2uF, which is specified on the datasheet (3.4uF).
Please let us confirm whether this 3.4uF input capacitance could some influence on the operation of this device.
2) When referring page 13 of SBVS012E, in case that input voltage is fallen below approximately 4V, the DCP will detect an under voltage condition.
However, when testing this sample, DCP010512DB seems to detect under voltage condition in case falled below 3.3V. In case 3.3 to 4V input, DCP010512DB tried to output, but this was result in failed.
Please let us know what is the correct operation in case of under voltage condition on this device.
We thank you in advance for your information.
Best regards,