Hi,
I want to use a buck regulator for cc2541. The regulator recommended by TI in the reference design is having a maximum input voltage of 3.9v. But I want to use a lipo battery so it's maximum voltage can go to 4.2v when it is fully charged. So I don't feel it is a good idea to use that regulator. Now I need to find a regulator which is having max input voltage >=4.2v and a very low quiescent current or power down mode swith because I am assuming the quiescent current can be a bottleneck. Now I found a regulator TPS82740 which have a quiescent curent < 500nA. But in ti website it is not not in stock, I called few distributor but they have no idea about this product.